Hello,
I have two camera-sensors on imx8mp ISP0 and ISP1 on two CSI ports
ls /dev
video1 (ISP0)
video2 (ISP1)
I cannot distinguish between those two. therefor I would like to add a udev rule to create fixed symbolic links.
Any idea how to do that?
Thank you,
已解决! 转到解答。
Hi Bio_TICFSL
Thank you for the feedback, but to be honest that did not help me at all.
Here is how I finally solved the problem.
Problem description again:
The two cameras appear as /dev/video1 and /dev/video2. Additionally ISI-CSI1 capture appears on /dev/video0.
As we cannot clearly identify which camera is mapped on CSI0 and CSI1, we need Udev Rules to set permanent links.
For example:
$ls /dev
video-isi-csi1 -> video0
video-isp-csi1 -> video1
video-isp-csi2 -> video2
To do this I added /lib/udev/rules.d/my_new.rules with this content:
CSI1 ISI Video Device
ACTION=="add", \
SUBSYSTEM=="video4linux", \
ATTR{name}=="mxc_isi.0.capture", \
DRIVERS=="mxc-md", \
SYMLINK+="video-isi-csi1"
CSI2 ISI Video Device
ACTION=="add", \
SUBSYSTEM=="video4linux", \
ATTR{name}=="mxc_isi.1.capture", \
DRIVERS=="mxc-md", \
SYMLINK+="video-isi-csi2"
CSI1 ISP Video Device
ACTION=="add", \
SUBSYSTEM=="video4linux", \
ATTR{name}=="viv_v4l20", \
DRIVERS=="vvcam-video", \
SYMLINK+="video-isp-csi1"
CSI2 ISP Video Device
ACTION=="add", \
SUBSYSTEM=="video4linux", \
ATTR{name}=="viv_v4l21", \
DRIVERS=="vvcam-video", \
SYMLINK+="video-isp-csi2"
Attribute "ATTR" of the node as well as parent nodes can be read using following commands:
udevadm info -a /dev/video0
udevadm info -a /dev/video1
udevadm info -a /dev/video2
Here is the output:
Udevadm info starts with the device specified by the devpath and then
walks up the chain of parent devices. It prints for every device
found, all possible attributes in the udev rules key format.
A rule to match, can be composed by the attributes of the device
and the attributes from one single parent device.
looking at device '/devices/platform/vvcam-video.0/video4linux/video1':
KERNEL=="video1"
SUBSYSTEM=="video4linux"
DRIVER==""
ATTR{dev_debug}=="0"
ATTR{index}=="0"
ATTR{name}=="viv_v4l20"
ATTR{power/control}=="auto"
ATTR{power/runtime_active_time}=="0"
ATTR{power/runtime_status}=="unsupported"
ATTR{power/runtime_suspended_time}=="0"
looking at parent device '/devices/platform/vvcam-video.0':
KERNELS=="vvcam-video.0"
SUBSYSTEMS=="platform"
DRIVERS=="vvcam-video"
ATTRS{driver_override}=="(null)"
ATTRS{power/control}=="auto"
ATTRS{power/runtime_active_time}=="0"
ATTRS{power/runtime_status}=="unsupported"
ATTRS{power/runtime_suspended_time}=="0"
looking at parent device '/devices/platform':
KERNELS=="platform"
SUBSYSTEMS==""
DRIVERS==""
ATTRS{power/control}=="auto"
ATTRS{power/runtime_active_time}=="0"
ATTRS{power/runtime_status}=="unsupported"
ATTRS{power/runtime_suspended_time}=="0"
Similar info can be gathered via (not 100% sure how to evaluate this though):
media-ctl --device /dev/media1 --print-topology
Hi Bio_TICFSL
Thank you for the feedback, but to be honest that did not help me at all.
Here is how I finally solved the problem.
Problem description again:
The two cameras appear as /dev/video1 and /dev/video2. Additionally ISI-CSI1 capture appears on /dev/video0.
As we cannot clearly identify which camera is mapped on CSI0 and CSI1, we need Udev Rules to set permanent links.
For example:
$ls /dev
video-isi-csi1 -> video0
video-isp-csi1 -> video1
video-isp-csi2 -> video2
To do this I added /lib/udev/rules.d/my_new.rules with this content:
CSI1 ISI Video Device
ACTION=="add", \
SUBSYSTEM=="video4linux", \
ATTR{name}=="mxc_isi.0.capture", \
DRIVERS=="mxc-md", \
SYMLINK+="video-isi-csi1"
CSI2 ISI Video Device
ACTION=="add", \
SUBSYSTEM=="video4linux", \
ATTR{name}=="mxc_isi.1.capture", \
DRIVERS=="mxc-md", \
SYMLINK+="video-isi-csi2"
CSI1 ISP Video Device
ACTION=="add", \
SUBSYSTEM=="video4linux", \
ATTR{name}=="viv_v4l20", \
DRIVERS=="vvcam-video", \
SYMLINK+="video-isp-csi1"
CSI2 ISP Video Device
ACTION=="add", \
SUBSYSTEM=="video4linux", \
ATTR{name}=="viv_v4l21", \
DRIVERS=="vvcam-video", \
SYMLINK+="video-isp-csi2"
Attribute "ATTR" of the node as well as parent nodes can be read using following commands:
udevadm info -a /dev/video0
udevadm info -a /dev/video1
udevadm info -a /dev/video2
Here is the output:
Udevadm info starts with the device specified by the devpath and then
walks up the chain of parent devices. It prints for every device
found, all possible attributes in the udev rules key format.
A rule to match, can be composed by the attributes of the device
and the attributes from one single parent device.
looking at device '/devices/platform/vvcam-video.0/video4linux/video1':
KERNEL=="video1"
SUBSYSTEM=="video4linux"
DRIVER==""
ATTR{dev_debug}=="0"
ATTR{index}=="0"
ATTR{name}=="viv_v4l20"
ATTR{power/control}=="auto"
ATTR{power/runtime_active_time}=="0"
ATTR{power/runtime_status}=="unsupported"
ATTR{power/runtime_suspended_time}=="0"
looking at parent device '/devices/platform/vvcam-video.0':
KERNELS=="vvcam-video.0"
SUBSYSTEMS=="platform"
DRIVERS=="vvcam-video"
ATTRS{driver_override}=="(null)"
ATTRS{power/control}=="auto"
ATTRS{power/runtime_active_time}=="0"
ATTRS{power/runtime_status}=="unsupported"
ATTRS{power/runtime_suspended_time}=="0"
looking at parent device '/devices/platform':
KERNELS=="platform"
SUBSYSTEMS==""
DRIVERS==""
ATTRS{power/control}=="auto"
ATTRS{power/runtime_active_time}=="0"
ATTRS{power/runtime_status}=="unsupported"
ATTRS{power/runtime_suspended_time}=="0"
Similar info can be gathered via (not 100% sure how to evaluate this though):
media-ctl --device /dev/media1 --print-topology
Hello,
Make sure that you have the cameras running and you can access to it before making a udev rule, then for making a udev visuallize which devices identification
su -c 'dmesg | tail | fgrep -i sd*'
The udevadm info process reports on a device (specified by the device path), then "walks" up the chain of parent devices.
Open a file called 80-local.rules in /etc/udev/rules.d and enter this code:
SUBSYSTEM=="you dvice", ACTION=="add", RUN+="/usr/local/bin/yourscritps.sh"
Regards