Hello,Community
Could you tell me if OpenCV uses GPU(2D/3D) or not on i.MX6.
Or tell me the method how to confirm it on i.MX6Sabre board.
Thank you!
ZongbiaoLiao
解決済! 解決策の投稿を見る。
Hi ZongbiaoLiao
yes it uses gpu, usage is described on
http://imxcv.blogspot.ca/2014/02/building-opencv-24x-for-freescales-imx6.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ZongbiaoLiao
yes it uses gpu, usage is described on
http://imxcv.blogspot.ca/2014/02/building-opencv-24x-for-freescales-imx6.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igorpadykov,
I'm confused on a comment in the link you provided:
http://imxcv.blogspot.ca/2014/02/building-opencv-24x-for-freescales-imx6.html
I saw Andre's comment ,the OpenCV seems couldn't take any advantage of iMX6 GPU. Not sure if I'm misunderstanding?
So far, I encountered facedetect uvc video performance issue both on iMX6Q Yocto 1.7 and Litb(linux BSP 4.1.0).
The symptom is CPU usage is around 99% and video capture from UVC(resolution is 720P) is very leg.
I'm not sure what can I improve. Thanks.
***********************************************************************************************************************************
Andre SilvaFebruary 4, 2015 at 2:06 AM
Hi Orion,
unfortunately it doesnt take any advantage of the gpu. OpenCV deals with CUDA and Full profile OpenCL, imx6 only supports the embedded profile. The performance is good as long you don´t use large images, I could run the face detection demo (modified to only detected front faces), on a 320x240 image at about 30fps, if I am not wrong.
seems this refers only to image detection and mentioned
in sect.5 AN4629 Fast Image Processing with i.MX 6 Series
http://cache.freescale.com/files/32bit/doc/app_note/AN4629.pdf
Hi Igorpadykov,
Could we have a way to enable OpenCL EP in OpenCV? (According to OpenCV SEPC, it seems need OpenCL full profile.)
Thanks.
according to sect.32.1 Overview i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
GPU module supports the following graphics APIs:
OpenCL 1.1 E
there is no way to change it as this is defined in hardware.
~igor