Yocto4.9.88:bitbake meta-toolchain-qt5 fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto4.9.88:bitbake meta-toolchain-qt5 fail

7,869 Views
yongheluo_hotma
Contributor III

Dear Sir,

     在编译meta-toolchain-qt5是,出现两个错误:

ERROR: meta-toolchain-qt5-1.0-r0 do_populate_sdk: Could not invoke dnf. Command '/home/yhluo/project_yocto/imx6_yocto_4.9.88_src/build-qt5/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/meta-toolchain-qt5/1.0-r0/recipe-sysroot-native/usr/bin/dnf -y -c /home/yhluo/project_yocto/imx6_yocto_4.9.88_src/build-qt5/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/meta-toolchain-qt5/1.0-r0/sdk/image/etc/dnf/dnf.conf --setopt=reposdir=/home/yhluo/project_yocto/imx6_yocto_4.9.88_src/build-qt5/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/meta-toolchain-qt5/1.0-r0/sdk/image/etc/yum.repos.d --repofrompath=oe-repo,/home/yhluo/project_yocto/imx6_yocto_4.9.88_src/build-qt5/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/meta-toolchain-qt5/1.0-r0/oe-sdk-repo --installroot=/home/yhluo/project_yocto/imx6_yocto_4.9.88_src/build-qt5/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/meta-toolchain-qt5/1.0-r0/sdk/image --setopt=logdir=/home/yhluo/project_yocto/imx6_yocto_4.9.88_src/build-qt5/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/meta-toolchain-qt5/1.0-r0/temp --nogpgcheck install nativesdk-packagegroup-sdk-host packagegroup-cross-canadian-imx6solosabresd nativesdk-packagegroup-qt5-toolchain-host' returned 1:
Added oe-repo repo from /home/yhluo/project_yocto/imx6_yocto_4.9.88_src/build-qt5/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/meta-toolchain-qt5/1.0-r0/oe-sdk-repo

......

Running transaction test
Error: Transaction check error:
file /opt/fsl-imx-fb/4.9.88-2.0.0/sysroots/x86_64-pokysdk-linux/environment-setup.d conflicts between attempted installs of nativesdk-cmake-3.8.2-r0.x86_64_nativesdk and nativesdk-qtbase-tools-5.9.4+git0+0d9208cecb-r0.x86_64_nativesdk

具体信息如下:

Host: Ubuntu 14.04, 64bit, (Virtulbox)

Yocto: 4.9.88 ga

Device: i.mx6solo

详细的log详见附件。

   谢谢!

  Yonghe.Luo

Labels (4)
10 Replies

5,661 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yonghe

one can try wit Ubuntu 14.04 and follow attached Yocto Guide

building image fsl-image-qt5-validation-imx shown on Table 1. i.MX Yocto project images.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,661 Views
yongheluo_hotma
Contributor III

Dear Igor,

      如果使用bitbake fsl-image-qt5-validation-imx -c populate_sdk,虽然可以编译出来一个1.3GB - 1.5GB的toolchain,但是,还是会缺少一些QT相关的工具。

     今天有重新编译了一下bitbake meta-toolchain-qt5, 仍然是存在同样的问题。

     因此,还是需要帮忙分析一下是什么原因,如何解决?

     谢谢!

    Yonghe.Luo

 

    

0 Kudos

5,661 Views
catia_han
NXP Employee
NXP Employee

Hi yonghe,

   Has this problem been solved? I met the same problem , and I  modified one line content in the ../sources/meta-qt5/recipes-qt/qt5/nativesdk-qtbase_git.bb  file. This line modified like below:

  

 fakeroot do_generate_qt_environment_file() { -    mkdir -p ${D}${SDKPATHNATIVE}/environment-setup.d/ +    install -d -m 755 ${D}${SDKPATHNATIVE}/environment-setup.d/      script=${D}${SDKPATHNATIVE}/environment-setup.d/qt5.sh        echo 'export PATH=${OE_QMAKE_PATH_HOST_BINS}:$PATH' > $script

 After modified,you can re-run $bitbake meta-toolchain-qt5,then the problem can be solved.

Best Regard

Catia Han

5,661 Views
muratboyar
Contributor I

Your solution has worked for my Yocto Rocko / iMX6 Solo Sabresd build. Thx a lot.

0 Kudos

5,662 Views
yongheluo_hotma
Contributor III

Dear Catia,

     非常感谢您的回复,这个问题已经解决。

     

      谢谢!

     Yonghe.Luo

0 Kudos

5,662 Views
csweagle
Contributor I

你好,我们也遇到了同样的问题,可以问一下是怎么解决的吗?

0 Kudos

5,662 Views
yongheluo_hotma
Contributor III

解决了。请参考上面的回复。

另外,网络上还有另外一种解决办法,具体链接我找不到了,你可以搜索一下。

0 Kudos

5,662 Views
yongheluo_hotma
Contributor III

Dear Igorpadykov

      昨天试了一下,使用bitbake fsl-image-qt5-validation-imx -c populate_sdk也是可以编译出完整的、包含QT5工具链的SDK。

      所以,可以不使用bitbake meta-toolchain-qt5 进行编译。

     谢谢!

     Yonghe.Luo

0 Kudos

5,662 Views
304338916
Contributor I

Hi Yonghe

 

我和您一样在bitbake meta-toolchain-qt5时,出现了一模一样的错误,你后来有没有解决这个问题呢?

我后来也尝试了下bitbake fsl-image-qt5-validation-imx -c populate_sdk,编译出的SDK里找不到Qt的编译工具qmake,只有.h和.lib文件,aarch64-poky-linux/usr/bin/qt5文件夹为空,请问您的结果也是这样么?

 

具体信息如下:

Host: Ubuntu 14.04, 64bit, (Virtulbox)

Yocto: 4.9.88 ga

Device: i.mx8mqevk

Best regards
Morey.Liu

0 Kudos

5,662 Views
yongheluo_hotma
Contributor III

Dear Morey,

    是的,我这边编译出来的包,/usr/bin/qt5也是空的。

    之前用bitbake meta-toolchain-qt5实际上编译是已经完成了,只是打包没有成功。可以找一下编译结果里面的/usr/bin/qt5是否有内容,是否拷贝过来用。

    另外,我这边也正在重新编译bitbake meta-toolchain-qt5。

    谢谢!

   Yonghe.Luo

0 Kudos