Yocto4.2 package have umet dependencies

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto4.2 package have umet dependencies

773 次查看
charleshuang
Senior Contributor II

Hi NXP,

I build imx-image-full fail in Yocto4.2, the error look like the package dependencies problem.

I am sure the jailhouse and cryptodev-module are already in "tmp/work".

The error logs as below. Any advice for this issue ?

Thanks !

 

===============================================

The following packages have unmet dependencies:
jailhouse : Depends: kernel-module-jailhouse-6.1.22-2620A1AIM36LIVC0005 but it is not installable
packagegroup-fsl-tools-testapps : Depends: cryptodev-module but it is not installable
E: Unable to correct problems, you have held broken packages.
 
ERROR: Logfile of failure stored in: /home/adv/BSP/imx8LBVC0005_2023-08-02/build_all/tmp/work/imx8ulprom2620a1-poky-linux/imx-image-full/1.0-r0/temp/log.do_rootfs.1369623
NOTE: recipe imx-image-full-1.0-r0: task do_rootfs: Failed
ERROR: Task (/home/adv/BSP/imx8LBVC0005_2023-08-02/sources/meta-imx/meta-sdk/dynamic-layers/qt6-layer/recipes-fsl/images/imx-image-full.bb:do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 11196 tasks of which 938 didn't need to be rerun and 1 failed.
 
Summary: 1 task failed:
  /home/adv/BSP/imx8LBVC0005_2023-08-02/sources/meta-imx/meta-sdk/dynamic-layers/qt6-layer/recipes-fsl/images/imx-image-full.bb:do_rootfs
Summary: There were 46 WARNING messages.
Summary: There was 1 ERROR message, returning a non-zero exit code.
 
 
0 项奖励
回复
3 回复数

755 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @charleshuang 

Can you try to clean all about these two packages: packagegroup-fsl-tools-testapps and cryptodev-module?

 

0 项奖励
回复

732 次查看
charleshuang
Senior Contributor II

Hi Zhiming_Liu,

Bad news ...

I try it, but the result is the same. 

0 项奖励
回复

725 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @charleshuang 

Please try to delete the build folder and rebuild it from begining..

0 项奖励
回复