Yocto on iMX6 Series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto on iMX6 Series

748 Views
chetansangli
Contributor I

Hi,

We are interested in bring up of Yocto on IMX6 Series for Automotive AVB, would like to know is there any Licensing issues with software ?

I mean do we need to buy firmware/driver/libraries specifically for audio or video or graphics parts to work ?

Thanks in advance

chetan

Tags (3)
0 Kudos
Reply
1 Reply

485 Views
art
NXP Employee
NXP Employee

The current Yocto BSPs for the i.MX6 series processors do not include any special features for AVB support. Any other drivers (including audio/video/graphics), included in the BSPs, can be used as is with no licensing limitations.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply