[Yocto] i.MX6 Play video failed for long run test on HDMI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Yocto] i.MX6 Play video failed for long run test on HDMI

709件の閲覧回数
charleshuang
Senior Contributor II

I play a AVI format vedio for long run test on HDMI, the system will crash.

1) AVI format vedio file:

  a) Video:

Resolution: 1280*720

Encode: H.264

Frame rate: 30/frames per second

  b) Audio:

Encode: Mpeg 1 layer 3

Channel: Stereo

Sample rat:44100 Hz

2) Play command on Yocto 3.10.17.1.0.2:

gst-launch playbin2 uri=file:////yocto_demo/2015_demo.avi video-sink="mfw_v4lsink device=/dev/video16" audio-sink="alsasink device=plughw:0"

3) Play command on Yocto 3.14.28.1.0.0:

  a) Gstreamer 1.x for an AVI file is as follows:

gst-launch-1.0 filesrc location=/yocto_demo/2015_demo.avi typefind=true ! video/x-msvideo ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! overlaysink demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! pulsesink

  b) A Gstreamer 0.10 AVI file playback example is as follows:

gst-launch filesrc location=/yocto_demo/2015_demo.avi typefind=true ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! imxv4l2sink demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! pulsesink

4) Reference file:

     a) hdmi_demo_audio.sh

          Link URL: https://www.dropbox.com/s/hqgnf0com6ksdsw/hdmi_demo_audio.sh?dl=0

     b) 2015_demo.avi

          Link URL: https://www.dropbox.com/s/cx6lkacr7z0opz0/2015_demo.avi?dl=0

Can you help me to solve this issue?

Thank you.

Best Regards,

Alex Cheng

ラベル(5)
0 件の賞賛
返信
1 返信

466件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you try other files? have the same issue? and pls upload the log file to check.

0 件の賞賛
返信