Hi,
I was checking at the Yocto hardknott release for some i.MX8m tests and I saw that there is "only" the support of QT4/QT5 in the meta-freescale/dynamic-layers.
Is the support of the i.MX GPU for QT6.x planned?
解決済! 解決策の投稿を見る。
yes, have this plan, new bsp would integrate the QT6 later, but I don't have detailed roadmap yet
*wrong reply*
yes, have this plan, new bsp would integrate the QT6 later, but I don't have detailed roadmap yet
Thanks for this quick answer.
I'm asking this question because we can already find some integration from third-party like Boundary Devices regarding boot2qt and I'm wondering if it should be complex to use this work to integrate the standard QT6 Layer on Yocto instead of using Boot2Qt.