Yocto hardknott : QT6.x support on meta-freescale

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto hardknott : QT6.x support on meta-freescale

Jump to solution
1,870 Views
frk
Contributor III

Hi,

I was checking at the Yocto hardknott release for some i.MX8m tests and I saw that there is "only" the support of QT4/QT5 in the meta-freescale/dynamic-layers.

Is the support of the i.MX GPU for QT6.x planned?

0 Kudos
1 Solution
1,865 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, have this plan, new bsp would integrate the QT6 later, but I don't have detailed roadmap yet

 

View solution in original post

3 Replies
1,859 Views
frk
Contributor III

*wrong reply*

0 Kudos
1,866 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, have this plan, new bsp would integrate the QT6 later, but I don't have detailed roadmap yet

 

1,857 Views
frk
Contributor III

Thanks for this quick answer.

I'm asking this question because we can already find some integration from third-party like Boundary Devices regarding boot2qt and I'm wondering if it should be complex to use this work to integrate the standard QT6 Layer on Yocto instead of using Boot2Qt.

0 Kudos