Hi,
Run dd command
$ sudo dd if=fsl-image-gui-imx28evk-20130417013203.rootfs.sdcard of=/dev/sdf bs=4M
171+0 records in
171+0 records out
717225984 bytes (717 MB) copied, 221.253 s, 3.2 MB/s
And boot from SD0, the system can't boot up, list debug message in blue below. Any idea to find what cause from?
U-Boot 2012.10-00994-g7e6c682 (Apr 17 2013 - 11:04:38) |
CPU: Freescale i.MX28 rev1.2 at 454 MHz
BOOT: SSP SD/MMC #0, 3V3
I2C: ready
DRAM: 128 MiB
MMC: MXS MMC: 0
MMC0: Command 8 timeout (status 0xe0384020)
*** Warning - bad CRC, using default environment
In: | serial |
Out: serial
Err: serial
Net: FEC0 [PRIME]
Warning: FEC0 using MAC address from net device
, FEC1
Warning: FEC1 using MAC address from net device
Hit any key to stop autoboot: 0
MMC0: Command 8 timeout (status 0xe02c4020)
reading boot.scr
** Unable to read "boot.scr" from mmc 0:2 **
reading uImage
2590572 bytes read
Booting from mmc ...
reading imx28-evk.dtb
** Unable to read "imx28-evk.dtb" from mmc 0:2 **
## Booting kernel from Legacy Image at 42000000 ...
Image Name: Linux-2.6.35.3-10.12.01+yocto+gc
Created: | 2013-04-17 2:03:22 UTC |
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: | 2590508 Bytes = 2.5 MiB |
Load Address: 40008000
Entry Point: 40008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.35.3-10.12.01+yocto+gc0879e9 (thomas@thomas-Linux) (gcc version 4.7.2 (GCC) ) #1 PREEMPT Wed Apr 17 10:03:12 CST 2013
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: Freescale MX28EVK board
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
Kernel command line: console=ttyAMA0,115200 root=/dev/mmcblk0p3 rw rootfstype=ext3 rootwait
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 124260k/124260k available, 6812k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB) | ||
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) | ||
DMA | : 0xfde00000 - 0xffe00000 ( 32 MB) | |
vmalloc : 0xc8800000 - 0xf0000000 ( 632 MB) | ||
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) | ||
modules : 0xbf000000 - 0xc0000000 ( 16 MB) | ||
.init : 0xc0008000 - 0xc0030000 ( 160 kB) | ||
.text : 0xc0030000 - 0xc0503000 (4940 kB) | ||
.data : 0xc0504000 - 0xc0542160 ( 249 kB) |
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
RCU-based detection of stalled CPUs is disabled. | |
Verbose stalled-CPUs detection is disabled. |
NR_IRQS:288
Console: colour dummy device 80x30
console [ttyAMA0] enabled
Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
regulator: core version 0.5
NET: Registered protocol family 16
regulator: vddd: 800 <--> 1575 mV at 1500 mV fast normal
regulator: vdddbo: 800 <--> 1575 mV fast normal
regulator: vdda: 1500 <--> 2275 mV at 1800 mV fast normal
vddio = 3380000, val=10
regulator: vddio: 2880 <--> 3680 mV at 3380 mV fast normal
regulator: overall_current: fast normal
regulator: vbus5v:
regulator: mxs-duart-1: fast normal
regulator: mxs-bl-1: fast normal
regulator: mxs-i2c-1: fast normal
regulator: mmc_ssp-1: fast normal
regulator: mmc_ssp-2: fast normal
regulator: charger-1: fast normal
regulator: power-test-1: fast normal
regulator: cpufreq-1: fast normal
i.MX IRAM pool: 124 KB@0xc8820000
usb DR wakeup device is registered
IMX usb wakeup probe
audit: cannot initialize inotify handle
bio: create slab <bio-0> at 0
SCSI subsystem initialized
Freescale USB OTG Driver loaded, $Revision: 1.55 $
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource mxs clock source
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Bus freq driver module loaded
IMX usb wakeup probe
usb h1 wakeup device is registered
audit: initializing netlink socket (disabled)
type=2000 audit(0.490:1): initialized
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
msgmni has been set to 242
alg: No test for stdrng (krng)
cryptodev: driver loaded.
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Console: switching to colour frame buffer device 100x30
mxs-duart.0: ttyAMA0 at MMIO 0x80074000 (irq = 47) is a DebugUART
mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0
Found APPUART 3.1.0
mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1
Found APPUART 3.1.0
mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2
Found APPUART 3.1.0
mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3
Found APPUART 3.1.0
mxs-auart.4: ttySP4 at MMIO 0x80072000 (irq = 116) is a mxs-auart.4
Found APPUART 3.1.0
brd: module loaded
loop: module loaded
i.MX GPMI NFC
NFC: Version 1, 8-chip GPMI and BCH
gpmi-nfc: probe of gpmi-nfc.0 failed with error 1
mxs-spi mxs-spi.0: Max possible speed 120000 = 120000000/2 kHz
mxs-spi mxs-spi.0: at 0x80014000 mapped to 0xF0014000, irq=84, bus 1, DMA ver_major 4
FEC Ethernet Driver
fec_enet_mii_bus: probed
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci: irq 93, io base 0x80080000
fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.0: irq 92, io base 0x80090000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mice: PS/2 mouse device common for all mice
input: mxs-kbd as /devices/platform/mxs-kbd.0/input/input0
input: MXS touchscreen as /devices/virtual/input/input1
MXS RTC driver v1.0 hardware v2.3.0
mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
Linux video capture interface: v2.00
mxs-pxp mxs-pxp.0: initialized
mxs watchdog: initialized, heartbeat 19 sec
mxs-mmc: MXS SSP Controller MMC Interface driver
mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96
dcp dcp.0: DCP crypto enabled.!
usbcore: registered new interface driver hiddev
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
mmc0: new high speed SD card at address 0002
mmcblk0: mmc0:0002 N/A 3.67 GiB (ro)
mmcblk0: p1 p2 p3
sgtl5000_hw_read: read reg error : Reg 0x00
Device with ID register 0 is not a SGTL5000
mxs-spdif mxs-spdif.0: MXS SPDIF Audio Transmitter
No device for codec mxs spdif
No device for DAI mxs spdif
No device for DAI mxs-saif
No device for DAI mxs-spdif
asoc: mxs spdif <-> mxs-spdif mapping ok
ALSA device list:
#0: mxs-evk (mxs spdif)
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:00:08 UTC (8)
VFS: Cannot open root device "mmcblk0p3" or unknown-block(179,3)
Please append a correct "root=" boot option; here are the available partitions:
b300 | 3850240 mmcblk0 driver: mmcblk |
b301 | 1024 mmcblk0p1 |
b302 | 10240 mmcblk0p2 |
b303 | 684032 mmcblk0p3 |
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,3)
Backtrace:
[<c0034110>] (dump_backtrace+0x0/0x10c) from [<c03ce4ac>] (dump_stack+0x18/0x1c)
r6:c0029a14 r5:c7459000 r4:c0543018 r3:00000002
[<c03ce494>] (dump_stack+0x0/0x1c) from [<c03ce694>] (panic+0x74/0xf0)
[<c03ce620>] (panic+0x0/0xf0) from [<c0008f14>] (mount_block_root+0x1d4/0x218)
r3:00000002 r2:00000001 r1:c7c27f48 r0:c0487dc4
[<c0008d40>] (mount_block_root+0x0/0x218) from [<c0009130>] (mount_root+0xe0/0x124)
[<c0009050>] (mount_root+0x0/0x124) from [<c00092e0>] (prepare_namespace+0x16c/0x1cc)
r5:c0029a29 r4:c0542418
[<c0009174>] (prepare_namespace+0x0/0x1cc) from [<c0008b14>] (kernel_init+0x12c/0x16c)
r5:c0028214 r4:c0028214
[<c00089e8>] (kernel_init+0x0/0x16c) from [<c004e490>] (do_exit+0x0/0x6c0)
r5:c00089e8 r4:00000000
Hello,Thomas,
According to above log messages, linux kernel can't find file system. the issue should be from from u-boot environment settings. Are you using u-boot to boot system ?
Regards,
Weidong
Hi Thomas/Weidong.
I have also see this issue but not only with gui-sdk images also with gui. After some (hard) resets, kernel finishes booting correctly. OtavioSalvador, I tag you so you are aware of this issue. From my side, I have done any debugging.