Yocto HDMI dispaly custom hardware issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto HDMI dispaly custom hardware issue

Jump to solution
872 Views
saurabh206
Senior Contributor III

Hi,

We are having custom hardware, We found one strange issue.

Yocto core-image-minimal build work perfectly with HDMI display, LVDS display is also works fine.

While fsl-image-fb build works find with LVDS display but With HDMI display set system hangs.

Any possible issue why hdmi display is not working with fsl-image-fb?

Labels (4)
Tags (3)
1 Solution
544 Views
saurabh206
Senior Contributor III

Hi

I was the HDMI CEC issue.

Thanks

Saurabh

View solution in original post

2 Replies
544 Views
gusarambula
NXP TechSupport
NXP TechSupport

At which point does the system hangs? Would you please provide more details on the error and if possible an error log? Perhaps the boot arguments are not correct for HDMI output, how are you changing the active framebuffer from the LVDS to tge HDMI?

0 Kudos
545 Views
saurabh206
Senior Contributor III

Hi

I was the HDMI CEC issue.

Thanks

Saurabh