Yocto 1.7 qt4e

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto 1.7 qt4e

744件の閲覧回数
LPs
Contributor III

Hi all,

  I'm trying to add to my basic recipe, a recipe based similar to core-image-minimal.

I want to add qt4e with the minimal impact to my rootfs.

I included  qt4-embedded to IMAGE_INSTALL_append of my new image.

I tried to extract SDK with command -c populate_sdk, but qmake is not exportend into the sdk package: it means I cannot setup a correct kit in QTCreator IDE.

How can I add qmake to the sdk?

ラベル(2)
0 件の賞賛
返信
1 返信

557件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I’m afraid that Freescale does not support QT code. However, you could refer to the following document from the Community:

Setting up Qt Creator to build for i.MX6


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信