Xserver modifications for imx-gpu-viv

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Xserver modifications for imx-gpu-viv

2,085 次查看
chaitanyad
Contributor I

Hello ,

          I'm integrating gstreamer1.0 on an imx6 solo based platform. My kernel version is linux-imx 3.10.17. However, my X server dosent start. I'm getting the following error :

                                        X: symbol lookup error: /usr/lib/xorg/modules/drivers/vivante_drv.so: undefined symbol: gcoHAL_QuerySeparated3D2D

gstreamer1.0 plugin "gst1.0-fsl-plugin" requires "imx-gpu-viv" . I made that change in xf86-video-imxfb-vivante_3.10.17-1.0.0.bb to indicate dependency on im-gpu-viv like this:

"DEPENDS += "virtual/xserver virtual/libx11 virtual/libgal-x11 imx-gpu-viv pixman"

The recipe gets compiled but I get the above error when X server starts. Am I missing in something?

Thanks,

Chaitanya

0 项奖励
回复
2 回复数

1,789 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Chaitanya,

Try to move to 3.10.53, this release integrate gstreamer 1.0.

Please check:

Integration of gstreamer1.0 on imx6dl platform

Regards

1,789 次查看
chaitanyad
Contributor I

Hello,

         Yes that can be done, but currently its not possible for us to move to 3.10.53. So is it absolutely not possible to go ahead with 3.10.17 and still solve the above issue?

Thanks,

Chaitanya Dhere 

0 项奖励
回复