Would like to know the GPU Version for the KK 4.4.2 android release with kernel 3.0.35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Would like to know the GPU Version for the KK 4.4.2 android release with kernel 3.0.35

1,625 Views
sunishm
Contributor I

Hi ,

I would like to know the GPU Version for the KK 4.4.2 android release with the Kernel-3.0.35 .

Is it the GPU version to 5.0.11p1 ??

As i see for KK 4

Thanks

Labels (1)
0 Kudos
Reply
4 Replies

1,363 Views
igorpadykov
NXP Employee
NXP Employee

Hi SUNISH

GPU  4.6.9 p12 version, as shown in attached

documents.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,363 Views
sunishm
Contributor I

Hi igor,

Thanks,

Looks like attachment is missing

Regards,

Sunish.M

0 Kudos
Reply

1,363 Views
igorpadykov
NXP Employee
NXP Employee

At.jpg

0 Kudos
Reply

1,363 Views
sunishm
Contributor I

Thanks igor

0 Kudos
Reply