Wiring up two parallel cameras on a I.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wiring up two parallel cameras on a I.MX6Q

Jump to solution
758 Views
benjaminblanton
Contributor II

I have two analog cameras running through two analog video decoders outputing 8-bit BT.656 with embedded syncs.  Reading through the I.MX6 it's very clear how to connect one 8-bit camera (DATA12-DATA19), but I only see one parallel IPU on the pinout.  Do I wire the other 8-bit stream in to pins DATA02-DATA11?

Thanks!

Ben

Labels (1)
0 Kudos
Reply
1 Solution
661 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ben

IPU2_CSI1 are multiplexed on EIM pads, as described in

Table 4-2. Muxing Options p.316 i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
662 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ben

IPU2_CSI1 are multiplexed on EIM pads, as described in

Table 4-2. Muxing Options p.316 i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
661 Views
benjaminblanton
Contributor II

Perfect.  thank you!

0 Kudos
Reply