Why are all of the sahara drivers written only for linux ?
Are they currently working on sahara drivers for the windows CE operating system ? Has anyone attempted to port the sahara drivers over to windows CE ?
Also could we possibly use some of the functions of sahara without implementing the whole system, for instance if we wanted to use redmemory within windows ce without hab etc.