Wichi defconfig i.Max6Q use?imx_v6_v7_defconfig can not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wichi defconfig i.Max6Q use?imx_v6_v7_defconfig can not work

2,410 次查看
wenfu
Contributor III

I'm use i.Max6Q, the Kernel source is downloaded form here(http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/?h=imx_4.1.15_2.0.0_ga).

make imx_v6_v7_defconfig

make

But it telsl me

"

arch/arm/mach-imx/built-in.o: In function `init_mmdc_lpddr2_settings':
platform-spi_imx.c:(.text+0x77ac): undefined reference to `imx6sll_lpddr2_freq_change'
drivers/built-in.o: In function `mxsfb_probe':
debugfs.c:(.text+0x459f4): undefined reference to `mxc_dispdrv_gethandle'
make: *** [vmlinux] Error 1

"

Do I got the wrong defconfig?

Wichi defconfig  i.Max6Q use?

2 回复数

1,219 次查看
wenfu
Contributor III

Yes, imx_v7_defconfig supports all mx6 SoCs.

1,219 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Thank you Wen Fu, just to add to the discussion, there is a bit more detail on this thread:

https://community.nxp.com/message/856437?commentID=856437#comment-856437 

Regards,

0 项奖励
回复