Why the LPDDR4 channel connection interchanged with i.MX8M Mini in the reference design?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why the LPDDR4 channel connection interchanged with i.MX8M Mini in the reference design?

ソリューションへジャンプ
1,641件の閲覧回数
m_c
Senior Contributor I

In data sheet, DRAM_AC04 <-> CK_t_A and DRAM_AC24 <-> CK_t_B, but in the reference design,  DRAM_AC04 <-> CK_t_B and DRAM_AC24 <-> CK_t_A?

pastedImage_1.png

pastedImage_2.png

ラベル(1)
0 件の賞賛
返信
1 解決策
1,513件の閲覧回数
art
NXP Employee
NXP Employee

In the i.MX8MMini EVK design, the LPDDR4 channels _A and _B are completely swapped with regard to the LPDDR4 chip. This is done for the PCB routing convenience.

Best Regards,

Artur

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,514件の閲覧回数
art
NXP Employee
NXP Employee

In the i.MX8MMini EVK design, the LPDDR4 channels _A and _B are completely swapped with regard to the LPDDR4 chip. This is done for the PCB routing convenience.

Best Regards,

Artur

0 件の賞賛
返信
1,513件の閲覧回数
siegfried_buerger
Contributor II

I am not really sure, but I´ve noticed:

If you do not connect the pins as in the reference design, there will be crossings at the end, in the routing.

So i think it´s just because it´s better for the layout.