hello.
I have faced a strange issues, that when I compiled the spi driver into the kernel, the PHY mdio can not get the chipID ex. got the value is 0xffffffff, but when I compile the spi driver to module, and disabled ecspi1, the network is ok.
Is there a iomux confict?
the following is the iomux define, pls tell me what's wrong?
ECSPI1:
FEC1:
Hi 国承 张
one can look at ecspi1 dts example
imx6ul-14x14-ddr3-arm2.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
probably one can try to rebuild all image from scratch.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------