Why BRILLO has been added in audio hal of IMX6 N?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why BRILLO has been added in audio hal of IMX6 N?

699 Views
hungeason
Contributor II

I check source code of audio hal ,and there is flag be add in Android N .

1.Why the flag be added?

2.what is the use case?

3.Does there is side effect if we disable BROLLO.

The commit message as below:

commit cf6a3e04a0177f878115b2b2e6c035eb573576cf
Author: fang hui <b31070@freescale.com>
Date: Tue Nov 24 18:24:51 2015 +0800

MA-7298 - [audioHAL]: unite code with brillo

To keep tinyalsa on brillo as original, modify HAL codes.
use macro BRILLO to distinguish.

Labels (1)
0 Kudos
Reply
2 Replies

623 Views
Yuri
NXP Employee
NXP Employee

Hello,

   BRILLO option relates to Android Things and should not be used with i.MX6 Android N.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

623 Views
hungeason
Contributor II

Hi,Yuri

The flag is related to Android thing,but the flag is enable in i.MX6 android N .

Does there is side effect if we disable BROLLO?

Thanks

Eason

0 Kudos
Reply