Which signal is the clock source for i.MX6's ENET_MDC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which signal is the clock source for i.MX6's ENET_MDC?

ソリューションへジャンプ
274件の閲覧回数
Ryo_Aoki
Contributor III

Hi NXP.

We are currently having a problem with i.MX6solo's ENET_MDC and are gathering information to resolve it.
Which signal is the clock source for i.MX6solo's ENET_MDC?
I checked the reference manual and can't find any information.
It would be nice if there was documentation showing the connection with PLL.

Best regards.

ラベル(1)
0 件の賞賛
返信
1 解決策
256件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Ryo_Aoki 

It's from enet module clock: ipg_clk, the name in device tree is IMX6SX_CLK_ENET.

 

It would be nice if there was documentation showing the connection with PLL.

-->I couldn't find such connection diagram

Best Regards

Zhiming

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
257件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Ryo_Aoki 

It's from enet module clock: ipg_clk, the name in device tree is IMX6SX_CLK_ENET.

 

It would be nice if there was documentation showing the connection with PLL.

-->I couldn't find such connection diagram

Best Regards

Zhiming

0 件の賞賛
返信
247件の閲覧回数
Ryo_Aoki
Contributor III

Hi Zhiming.

Thank you for your reply.
However, I am targeting i.MX6solo, not i.MX6SX.
Is the clock source ipg_clk for i.MX6solo as well?

And can the clock source to this ENET_MDC be a different clock source than ipg_clk?
I was assuming that PLL6, for example, was being used.

Best regards.

0 件の賞賛
返信