Hi,
For i.MX28 Evaluation Kit (MCIMX28EVKJ: i.MX28 Evaluation Kit) which JTAG will be best supported. Does I.MX28 supports ARM-USB-TINY-H (ARM-USB-TINY-H)
已解决! 转到解答。
Hi Ganesh
yes i.MX28 supports it.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
1.
Please refer to the following summary link, which contains information about recommended tools, examples, available BSPs.
2.
Basically any JTAG tool, supporting ARM926 may be applied with i.MX28.
3.
To debug, using JTAG, we must enter special boot mode (Wait JTAG connection).
To debug the i.MX28/23, you must boot it in boot mode 6. In this mode, the boot ROM will enable
the JTAG pins and go into a two- instruction infinite loop, waiting for the debugger to release it.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ganesh
yes i.MX28 supports it.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------