Whether iMX6S support LPDDR2 or LPDDR3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whether iMX6S support LPDDR2 or LPDDR3?

Jump to solution
902 Views
DonnyChiu
Contributor II

Just want to confirm whether iMX6solo support LPDDR2 or LPDDR3.

Because somehow the website says 32 bit LP-DDR3/LV-DDR3 under Features -> Memory section

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/arm-mcus-and-mpus/i....

but on block diagram and datasheet, it says DDR3, low voltage DDR3, LPDDR2.

So, please update the webpage if the information is wrong.

Labels (1)
0 Kudos
Reply
1 Solution
803 Views
igorpadykov
NXP Employee
NXP Employee

Hi Donny

it supports LPDDR2, not LPDDR3. Image on mentioned link

"i.MX 6Solo Multimedia Applications Processor Block Diagram"

describes "x32 LP-DDR2/DDR3/LV-DDR3",

there is no reference to LPDDR3.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
803 Views
DonnyChiu
Contributor II

For your information, this is where it mentioned LPDDR3 on the web.

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/arm-mcus-and-mpus/i....

iMX6S Memory.png

0 Kudos
Reply
804 Views
igorpadykov
NXP Employee
NXP Employee

Hi Donny

it supports LPDDR2, not LPDDR3. Image on mentioned link

"i.MX 6Solo Multimedia Applications Processor Block Diagram"

describes "x32 LP-DDR2/DDR3/LV-DDR3",

there is no reference to LPDDR3.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply