Where to find SCU definitions for the i.MX8QM and i.MX8QX silicons?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where to find SCU definitions for the i.MX8QM and i.MX8QX silicons?

809 次查看
zee_z
Contributor III

Hello NXP support,

I am looking to redefine some i.MX8QM clock usages, namely the next SCU RPC call poses the vital interest to me:

in kernel_imx/drivers/clk/imx/clk-imx8qxp.c the imx_clk_scu2() call shown below:

imx_clk_scu2("mipi0_dsi_phy_clk", mipi_sels, ARRAY_SIZE(mipi_sels), IMX_SC_R_MIPI_0, IMX_SC_PM_CLK_PHY);

Where the params are:

[0] "mipi0_dsi_phy_clk" ==> resource, my best guess is:

uboot-imx/include/dt-bindings/clock/imx8qm-clock.h
846:#define IMX8QM_MIPI0_DSI_PHY_CLK 797

[1] mipi_sels, defined in kernel_imx/drivers/clk/imx/clk-imx8qxp.c

static const char *mipi_sels[] = {
"clk_dummy",
"clk_dummy",
"mipi_pll_div2_clk",
"clk_dummy",
"clk_dummy",
};

Where the unknown parameter to me is: "mipi_pll_div2_clk" (this is why I need these SCU FW definitions, since I need/should put there another divider)!

[2] ARRAY_SIZE(mipi_sels) = 5

[3] IMX_SC_R_MIPI_0, defined as resource in include/dt-bindings/firmware/imx/rsrc.h

#define IMX_SC_R_MIPI_0 393

[4] IMX_SC_PM_CLK_PHY, defined as clock in kernel_imx/include/dt-bindings/firmware/imx/rsrc.h

#define IMX_SC_PM_CLK_PHY 3 /* Phy clock */

_______

Any ideas where I can find these SCU FW definitions?

(I am using the following manual, not able to find them there: i.MX 8DualX/8DualXPlus/8QuadXPlus Applications Processor Reference Manual, Rev. 0, 05/2020. Maybe these values are defined in some other manual... In which?)

Is there any other method how to change the mipi0_dsi_phy_clk freq?

Thank you,

Zee

 

标记 (2)
0 项奖励
回复
1 回复

753 次查看
zee_z
Contributor III

I realize that I am a bit lost in this all i.MX8QM clocking tree Minotaur's maze... I apologize for this!

Actually, what I need to do is the following:

From:

adb_shell: / # cd /sys/kernel/debug/clk
adb_shell: /sys/kernel/debug/clk # cat clk_summary

...[snap]...

mipi_pll_div2_clk 2 2 0 432000000 0 0 50000
mipi0_dsi_rx_esc_clk 0 0 0 72000000 0 0 50000
mipi0_dsi_tx_esc_clk 1 1 0 18000000 0 0 50000
mipi0_dsi_phy_clk 1 1 0 27000000 0 0 50000
mipi1_dsi_phy_clk 0 0 0 27000000 0 0 50000

I need to increase mipi_pll_div2_clk to at least from (27 MHz x 16) to (27 MHz x 24 or 32) to get the higher resolution for the MIPI0_DSI link. Since the resolution I need, covered by mipi_pll_div2_clk 2 2 0 432000000 0 0 50000 is not supported (2880 x 720).

How I can increase this clock to cover the following from the dts tree?

panel-timing {
        clock-frequency = <137000000>;
        hactive = <2820>;
        vactive = <720>;
        ...[snap]...
};

Thank you,

Zee

 

标记 (2)
0 项奖励
回复