Where to find CCM_CSCDR3 register in Linux L3.10.53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where to find CCM_CSCDR3 register in Linux L3.10.53

926件の閲覧回数
dipalidhumal
Contributor I

Hi,

We are using i.MX6DL- (MCIMX6U8DVM10AC).

We need to modify CCM_CSCDR3 register values.

Please let us know where to get this register in Linux L3.10.53 from freescale.

Please let me for more information.

Regards,

Dipali

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

797件の閲覧回数
saurabh206
Senior Contributor III

Hi Dipali,

You can use memtool utility to modify register.

If you have yocto setup available than you can generate using bitbake imx-test.

Thanks

Saurabh

0 件の賞賛
返信

797件の閲覧回数
dipalidhumal
Contributor I

Hi,

We don't want to try this option with memtool utility.

We have to make it in Linux.

Please see below file and tell us the steps and procedures to be changed.

./arch/arm/mach-imx/clk-vf610.c:#define CCM_CSCDR3        (ccm_base + 0x1c)

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI0_EN] = imx_clk_gate("qspi0_en", "qspi0_sel", CCM_CSCDR3, 4);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI0_X4_DIV] = imx_clk_divider("qspi0_x4", "qspi0_en", CCM_CSCDR3, 0, 2);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI0_X2_DIV] = imx_clk_divider("qspi0_x2", "qspi0_x4", CCM_CSCDR3, 2, 1);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI0_X1_DIV] = imx_clk_divider("qspi0_x1", "qspi0_x2", CCM_CSCDR3, 3, 1);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI1_EN] = imx_clk_gate("qspi1_en", "qspi1_sel", CCM_CSCDR3, 12);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI1_X4_DIV] = imx_clk_divider("qspi1_x4", "qspi1_en", CCM_CSCDR3, 8, 2);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI1_X2_DIV] = imx_clk_divider("qspi1_x2", "qspi1_x4", CCM_CSCDR3, 10, 1);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_QSPI1_X1_DIV] = imx_clk_divider("qspi1_x1", "qspi1_x2", CCM_CSCDR3, 11, 1);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_DCU0_EN] = imx_clk_gate("dcu0_en", "dcu0_sel", CCM_CSCDR3, 19);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_DCU0_DIV] = imx_clk_divider("dcu0_div", "dcu0_en", CCM_CSCDR3, 16, 3);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_DCU1_EN] = imx_clk_gate("dcu1_en", "dcu1_sel", CCM_CSCDR3, 23);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_DCU1_DIV] = imx_clk_divider("dcu1_div", "dcu1_en", CCM_CSCDR3, 20, 3);

./arch/arm/mach-imx/clk-vf610.c:    clk[VF610_CLK_NFC_PRE_DIV] = imx_clk_divider("nfc_pre_div", "nfc_en", CCM_CSCDR3, 13, 3);

Regards,

Dipali

0 件の賞賛
返信

797件の閲覧回数
art
NXP Employee
NXP Employee

The listing you've provided is for VF6 series Vybrid controllers platform. Try

to find the same for MX6DL platform. Also, check the corresponding device tree file:

arch/arm/boot/dts/imx6dl.dtsi


Have a great day,
Artur

0 件の賞賛
返信

797件の閲覧回数
dipalidhumal
Contributor I

Hi Artur,

Thanks.

We have gone through the dtsi file as you mentioned and could not find any reference to CCM_CSCDR3.

PFB listing for imx processor which is the only reference regarding this register we found in the kernel code.

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3        (MX51_CCM_BASE + 0x3C)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_HSI2C_CLK_PRED_OFFSET        (16)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_HSI2C_CLK_PRED_MASK        (0x7 << 16)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_HSI2C_CLK_PODF_OFFSET        (9)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_HSI2C_CLK_PODF_MASK        (0x3F << 9)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_FIRI_CLK_PRED_OFFSET        (6)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_FIRI_CLK_PRED_MASK        (0x7 << 6)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_FIRI_CLK_PODF_OFFSET        (0)

./arch/arm/mach-imx/crm-regs-imx5.h:#define MXC_CCM_CSCDR3_FIRI_CLK_PODF_MASK        (0x3F)

Is it applicable to i.MXDL? If you have more information then share it with us.

Regards,

Dipali

0 件の賞賛
返信