Where is L3.10.17_1.0.2_SOURCE_BSP available for download ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is L3.10.17_1.0.2_SOURCE_BSP available for download ?

768 Views
thierrybultel
Contributor II

Hi,

On the dowload page, there are L3.0.101_4.1.1_SOURCE_BSP and L3.0.101_4.1.1_SOURCE_BSP but not L3.10.17_1.0.2_SOURCE_BSP

I am not using Yocto but buildroot, and I need

firmware-imx-xx.gz, xserver-xorg-video-imx-viv-xx.tar.gz ... where can I find them please ?

Regards

Thierry

Labels (1)
0 Kudos
Reply
2 Replies

641 Views
thierrybultel
Contributor II

Thanks !

0 Kudos
Reply

641 Views
Yuri
NXP Employee
NXP Employee

  The sources are loaded from repositories. Please use Release notes in


http://cache.freescale.com/files/32bit/doc/support_info/IMX6YOCTOPATCHRN.pdf

Demo images :

https://www.freescale.com/webapp/Download?colCode=L3.10.17_1.0.2_iMX6QDLS_BUNDLE&appType=license&loc...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply