Where did the nice window manager go in 4.9.88_2.0.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where did the nice window manager go in 4.9.88_2.0.0?

ソリューションへジャンプ
973件の閲覧回数
dennis3
Contributor V

The demo SD card I got with my i.mx7d board has kernel 4.1.15.  Linux boots and then loads an Xsession capable of calibrating the touch screen, connecting to a wireless network, running x11vnc, some demos etc.

I built a 4.9.88_2.0.0 image with the yocto build system (Also tried the prebuilt images to make sure) and Xorg is pretty much stock/empty.  It won't start without modifying xorg.conf because the Driver line specifying vivante fails to load any drivers.  If I remove that and just use Driver "fbdev" I can get it to launch Xorg.  From there I can launch a window manager and X programs.  I found several of the demos, a window manager and other odds and ends.  

Am I missing a layer somewhere that contains all the configuration details to launch everything in a nice way?  There seem to be other common configuration files not included in the build.. example /etc/network/interfaces

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
808件の閲覧回数
dennis3
Contributor V

After further comparisons with the older image, it seems this is actually just an issue with Xorg not starting due to the missing vivante driver listed in the xorg.conf.  The rest of the matchbox application links and samples are in fact available if X starts correctly at boot.  

Touchscreen calibration/input doesn't seem to be working though... on to the next problem. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
809件の閲覧回数
dennis3
Contributor V

After further comparisons with the older image, it seems this is actually just an issue with Xorg not starting due to the missing vivante driver listed in the xorg.conf.  The rest of the matchbox application links and samples are in fact available if X starts correctly at boot.  

Touchscreen calibration/input doesn't seem to be working though... on to the next problem. 

0 件の賞賛
返信
808件の閲覧回数
weidongzhou
Contributor I

Dennis,

xorg changes touchscreen support from xinput-calibrator to TransformationMatrix. You may check if libinput hit your issue.

Weidong

0 件の賞賛
返信