Where can we download aac codec package for Android 5.0.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can we download aac codec package for Android 5.0.0?

1,440 Views
m_c
Senior Contributor I

In <Android L5.0.0_1.0.0 GA Release>, there is an link for aac codec package for Android 5.0.0, but we can't download it. Where can we download it?

https://www.freescale.com/webapp/Download?colCode=IMX6-L500-100-AACP-CODEC-CODA&appType=license&loca...

Labels (2)
Tags (4)
2 Replies

956 Views
b36401
NXP Employee
NXP Employee

Here is the link:

http://www.nxp.com/webapp/Download?colCode=IMX6-L500-100-AACP-CODEC-CODA

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

956 Views
danny_lu
Contributor II

Hi Victor,

Is there any license issue using this codec package I should be aware of?

Thank you

Danny

0 Kudos