Hi everyone:
As the title, now I have a i.MX53QSB and a "MCIMXHDMICARD" which can output with HDMI signal BOARD.
I have two LCD panels, resolution are 1024*600 and 1280*800
I want to know where Could I set the different resolution to match above resolution
coz the document told the HDMI just support 720p(1280*720) and 1080p(1920*1080) resolution (the file is shown as attached. file name: Release Notes r4.2.pdf) page15
if anyone knows that ,,, just help thx
Might I need to told detail
My operation system is android 2.3.4 which is use ADENEO (http://www.adeneo-embedded.com/en/Products/Board-Support-Packages/F...) provided BSP.
Now I have already setup the system successfully, afterward want to
use HDMI daughter card to output two resolution (1024*600 & 1280*800)
Therefore, which file do I need to modify the "struct" under /src/kernel-imx/arm/arch/........like to add
"static struct fb_videomode video_modes[]
= { ...
{
"1080P60", 60, 1920, 1080, 7692,
100, 40,
30, 3,
10, 2,
0,
FB_VMODE_NONINTERLACED,
0,},
" or I don't need to modify any "struct".
Just after enable HDMI, the sil902x driver will try to fetch video modes by reading EDID code, if succeed, these panel will operating normally.
really thx anyone help kindly~~
Hello Lan Bo Wei,
This other forum may be helpful to you. "Configuring the i.MX53 QSB HDMI Output Resolution"
Also a helpful tip if you have access to google search: In the google search bar, you can type site:imxcommunity.org i.MX53 HDMI or any other related tags instead of HDMI and it will present all the forums with that keyword.