When i.MX6 AUDMUX uses both Normal Mode and Internal Network Mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When i.MX6 AUDMUX uses both Normal Mode and Internal Network Mode.

ソリューションへジャンプ
592件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6Q AUDMUX.

They want to confirm whether Port 1 and Port 2 output data during Port 7 output data in the following case.

Port 1 --(Normal Mode for I2S)--> Port 6

Port 2 --(Normal Mode for I2S)--> Port 5

Port 7 --+--(Internal Network Mode)--> Port 4

              |--(Internal Network Mode) --> Port 3

In this case, if Port 1 and Por 2 are in Internal Network Mode, these are not able to output data during Port 7 output data.

But these are in Normal Mode, it is no problem, right?

Best Regards,

Satoshi Shimoda

ラベル(6)
タグ(1)
0 件の賞賛
1 解決策
421件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think you are right, Port 1 and Port 2 should be used in

Normal Mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
422件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think you are right, Port 1 and Port 2 should be used in

Normal Mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛