Hi community,
Our partner have a question about i.MX6Q AUDMUX.
They want to confirm whether Port 1 and Port 2 output data during Port 7 output data in the following case.
Port 1 --(Normal Mode for I2S)--> Port 6
Port 2 --(Normal Mode for I2S)--> Port 5
Port 7 --+--(Internal Network Mode)--> Port 4
|--(Internal Network Mode) --> Port 3
In this case, if Port 1 and Por 2 are in Internal Network Mode, these are not able to output data during Port 7 output data.
But these are in Normal Mode, it is no problem, right?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hi Satoshi
I think you are right, Port 1 and Port 2 should be used in
Normal Mode.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
I think you are right, Port 1 and Port 2 should be used in
Normal Mode.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------