When do we run the i.MX6 DDR Stress tool and what should be the settings of the boot pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When do we run the i.MX6 DDR Stress tool and what should be the settings of the boot pins

ソリューションへジャンプ
730件の閲覧回数
atillametetured
Contributor V

Hi,

As the title suggests, can I run DDR Test Tool over USB in a fresh Board? What should be the boot settings? Should they be set to serial downloader since it will be using the USB connection, and by USB connection, we are talking about the USB OTG port right?

Regards,

Mete

ラベル(2)
1 解決策
619件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mete

right, they should be set to serial downloader and use USB OTG port.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
620件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mete

right, they should be set to serial downloader and use USB OTG port.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

619件の閲覧回数
atillametetured
Contributor V

Thanks Igor.

Regards,

Mete

0 件の賞賛
返信