When do we run the i.MX6 DDR Stress tool and what should be the settings of the boot pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

When do we run the i.MX6 DDR Stress tool and what should be the settings of the boot pins

跳至解决方案
669 次查看
atillametetured
Contributor V

Hi,

As the title suggests, can I run DDR Test Tool over USB in a fresh Board? What should be the boot settings? Should they be set to serial downloader since it will be using the USB connection, and by USB connection, we are talking about the USB OTG port right?

Regards,

Mete

标签 (2)
1 解答
558 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mete

right, they should be set to serial downloader and use USB OTG port.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
559 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mete

right, they should be set to serial downloader and use USB OTG port.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

558 次查看
atillametetured
Contributor V

Thanks Igor.

Regards,

Mete

0 项奖励