What to do with CSI0_DATA_EN input when connection camera without this signal.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What to do with CSI0_DATA_EN input when connection camera without this signal.

跳至解决方案
3,333 次查看
camz
Contributor I

I am looking for information on what to do with the CSI0_DATA_EN input on the i.MX6 when connecting a camera that only provides PIXCLK, HSYNC, and VSYNC.

The CSI0 interface will be configured for greyscale/generic 16-bit data mode.

Cheers,

Camz.

标签 (2)
0 项奖励
回复
1 解答
3,108 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

you can tie physical pin high or low or left unconnected (then enable

internal pin pull-up), necessary polarity can be changed

with IPUx_CSIx_SENS_CONF bit CSIx_DATA_EN_POL.

~igor

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,108 次查看
camz
Contributor I

Perfect, thank you.

0 项奖励
回复
3,108 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

CSI0_DATA_EN input should be active for normal operation.

Usually in such cases this signal is selected with IOMUX

to some pad, with enabled pad pull-up. Also polarity can be changed

with IPUx_CSIx_SENS_CONF bit CSIx_DATA_EN_POL.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,108 次查看
camz
Contributor I

I guess I wasn't as clear with my question as I could have been.  I am not looking for a software answer, this was not a question about how to configure the iomux.  This was a hardware connection question.

I have a camera that provides data, pixel clock, h-sync, and v-sync signals (actually the sync signals are also called frame enable and line enable).  It *does not* provide a data enable signal. 

The question is what to do with the physical pin that would normally be connected via the iomux to data enable?

Should it be left unconnected?   Tied high or low?  Should it be connected to the h-sync / line enable signal?  Should it be connected to the v-sync / frame enable signal?

Cheers,

Camz.

0 项奖励
回复
3,109 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

you can tie physical pin high or low or left unconnected (then enable

internal pin pull-up), necessary polarity can be changed

with IPUx_CSIx_SENS_CONF bit CSIx_DATA_EN_POL.

~igor

0 项奖励
回复