What's MMDC PHY ODT control register(MMDC_MPODTCTRL)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What's MMDC PHY ODT control register(MMDC_MPODTCTRL)?

535 次查看
kwangbogham
Contributor II

Dear everyone,

I'm preparing something to do the DDR stress test for i.MX6 solo lite with DDR3.

The attached document is provided from Freescale field engineer and  is to make Aid file before test starts out.

As you know in the attached file, there are some "MMDC Control Parameter" to set the ODT.

Here are some question.

1. What's an affection of four parameter (ODT3_IN_RES, ODT2_IN_RES, ODT1_IN_RES and ODT0_INT_RES) in MPODTCTRL register?

    which one? just only DQ(data line) or not?

   Maybe i think that four parmeter make an affection to DQ line.

2. If four parameter is for only DQ(data line),

    What we are interfacing with i.mx6 solo lite is DDR3 memory.

    it's 16bit data bus.

    I don't know that i must control and set which parameter of above four parameter?

    plz, let me know that i must to control which one.

3. Why is there four parameter ?

    Plz, let me explain in more detailed what's the purpose each other?

4. In the attached file, "control bit setting' is default 1(decimal). it means that Rtt resistor is 120 ohm.

    Is it recommandation value or not?

  

Best & Regards,

Kwangbog HAM

标签 (1)
0 项奖励
1 回复

364 次查看
igorpadykov
NXP Employee
NXP Employee

Hi kwangbog

1. yes this is data lines, per byte control

2.3. recommended to run ibis modelling (check IMX6DQ6SDLHDG

Chapter 9 Understanding the IBIS Model) to choose best option

4. one can start with script for i.MX6SL EVK,

MX6SL_EVK_DDR3_v0.5.inc i.MX 6Series Platform SDK

then change it for custom board (if necessary), based on DDR test results

i.MX6 DDR Stress Test Tool V1.0.3

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励