What is the specifications to power up hdmi to vga signals with imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the specifications to power up hdmi to vga signals with imx6

644件の閲覧回数
narasimhuluorug
Contributor III

Hello,

Is there any power limitations which is to power up the display monitor with hdmi to vga conversions ?

Thanks & Regards

narasimha

0 件の賞賛
返信
1 返信

573件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi narasimha

there are no special limitations, in general first should be powered

processor, then external devices.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信