I'm running with SABRESDB in preparation for my custom hardware.
My custom hardware core is similar to SABRESDB; but I still wanna make sure I know how to build/modify the .dtb file.
I'm currently reading through the kernel's Documentation/devicetree/usage-mode.txt and also http://devicetree.org/Device_Tree_Usage,
are these documentation sources the correct place to be reading up on the FDT stuff used with iMX6/SabreSDB or is there
additional/other places to get better acquainted with this?
Thanks in advance,
Ed
EDIT---
Perhaps a more fundamental question is: will I need to modify the .dts file for custom iMX6 hardware or is this file something that describes the SOC/CPU and its IO independent of the circuitry around the SOC?
解決済! 解決策の投稿を見る。
Ed,
A .dts file describes a particular board. You can start with imx6qdl-sabresd.dtsi, for example and adapt it to your own board.
You can see how other mx6 boards are supported in device tree: ls -al arch/arm/boot/dts/imx6*
Regards,
Fabio Estevam
Ed,
A .dts file describes a particular board. You can start with imx6qdl-sabresd.dtsi, for example and adapt it to your own board.
You can see how other mx6 boards are supported in device tree: ls -al arch/arm/boot/dts/imx6*
Regards,
Fabio Estevam
Fabio,
Ok, I've been looking at this since I posted the question. I see the .dts file is processed by 'dtc' (device-tree-compiler i assume?)
to generate the .dtb file. Does this binary translate into runtime initialization in the kernel somewhere?
One other question...
I noticed an option in kernel menuconfig: "Use appended device tree blob to zImage (EXPERIMENTAL)".
Does this do what it implies; thus eliminating the need to download the separate .dtb file and using the 3-argument bootm command?
Thanks much,
Ed
Hi Ed,
Yes, when you run "make imx6q-sabresd.dtb' , the dts file is converted to the dtb binary.
Just replied in more details about the appended device tree in another thread.
Regards,
Fabio Estevam