What is the minimum safe voltage for iMX6 VDD_ARM_IN when using the PF0100?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the minimum safe voltage for iMX6 VDD_ARM_IN when using the PF0100?

Jump to solution
1,305 Views
nathanpalmer
Contributor IV

I know that the Data Sheet for the iMX6SL says that the minimum voltage for the VDD_ARM_IN rail is 0.95V @ 400MHz but I am concerned about using this value with the PF0100 due to voltage ripple.  My question is, what is the minimum SAFE value of VDD_ARM_IN when supplying the rail from an external PF0100 PMIC (with a +- 25mV accuracy and 10mV ripple)? 

The reason for my confusion is that the on-chip PMU says that it provides ripple-rejection and I want to make sure I am interpreting the data sheet correctly, since I am bypassing the internal LDOs to save power.  I am concerned that I will not save much power after all if I have to bump up the SW1AB voltage on the PF0100 to account for ripple and ensure proper operation across temperature, so I would like to keep it at 0.95V if it is safe.

Want to ensure this mode will operate correctly across temperature and process variance:

Setup:

iMX6SL @ 400 MHz, Internal PMU: VDD_ARM_IN = internal bypass mode (TARG=0x1F)

PF0100 SW1AB connected to VDD_ARM_IN; Configured via SPI to 0.95V with boot code

Labels (2)
0 Kudos
Reply
1 Solution
842 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

"ripple-rejection" means rejection at PMIC input (VIN).

PMIC output voltages accuracy are given in datasheet.

So you are right - one needs to increase PMIC output to

compensate PMIC output voltages accuracy and ripple.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
843 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

"ripple-rejection" means rejection at PMIC input (VIN).

PMIC output voltages accuracy are given in datasheet.

So you are right - one needs to increase PMIC output to

compensate PMIC output voltages accuracy and ripple.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply