What is the minimum safe voltage for iMX6 VDD_ARM_IN when using the PF0100?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the minimum safe voltage for iMX6 VDD_ARM_IN when using the PF0100?

跳至解决方案
1,732 次查看
nathanpalmer
Contributor IV

I know that the Data Sheet for the iMX6SL says that the minimum voltage for the VDD_ARM_IN rail is 0.95V @ 400MHz but I am concerned about using this value with the PF0100 due to voltage ripple.  My question is, what is the minimum SAFE value of VDD_ARM_IN when supplying the rail from an external PF0100 PMIC (with a +- 25mV accuracy and 10mV ripple)? 

The reason for my confusion is that the on-chip PMU says that it provides ripple-rejection and I want to make sure I am interpreting the data sheet correctly, since I am bypassing the internal LDOs to save power.  I am concerned that I will not save much power after all if I have to bump up the SW1AB voltage on the PF0100 to account for ripple and ensure proper operation across temperature, so I would like to keep it at 0.95V if it is safe.

Want to ensure this mode will operate correctly across temperature and process variance:

Setup:

iMX6SL @ 400 MHz, Internal PMU: VDD_ARM_IN = internal bypass mode (TARG=0x1F)

PF0100 SW1AB connected to VDD_ARM_IN; Configured via SPI to 0.95V with boot code

标签 (2)
0 项奖励
回复
1 解答
1,269 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

"ripple-rejection" means rejection at PMIC input (VIN).

PMIC output voltages accuracy are given in datasheet.

So you are right - one needs to increase PMIC output to

compensate PMIC output voltages accuracy and ripple.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,270 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

"ripple-rejection" means rejection at PMIC input (VIN).

PMIC output voltages accuracy are given in datasheet.

So you are right - one needs to increase PMIC output to

compensate PMIC output voltages accuracy and ripple.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复