What is the maximum input voltage for VLDO34, in MC32PF3000A2EP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the maximum input voltage for VLDO34, in MC32PF3000A2EP

635 次查看
logeshs
Contributor II

Hi,

We are using PMIC MC32PF3000A2EP in our design with MCIMX7D3EVK10SD.

 

1: What is the maximum input voltage for VLDO34? There are two different specs available in datasheet. At page 25, it shows 2.8V to 3.6V. In Figure 5 Power map, VLDO4 input is connected to VIN and says 4.5V(Typ).

Please let us know which one should I refer.

Thanks

Logesh

标签 (1)
0 项奖励
2 回复数

495 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  According to Table 3 (Absolute maximum voltage ratings) of the PMIC Datasheet (PF3000,
Rev. 9.0, 8/2017 ), voltage range for VLDO34IN  is -0.3 to 3.6 (V)

https://www.nxp.com/docs/en/data-sheet/PF3000.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

495 次查看
marcfigliuolo
Contributor I

Hello Yuri

When I look at the i.MX7Sabre EVB schematic, VLDO34IN is supplied 3.7V and when I look at the PF3000 EVB, VLDO34IN is supplied with Vin which is also 4.4V. Are you sure that the datasheet is correct?

Many thanks for your efforts.

Greets Marc

0 项奖励