What is the internal resistance of the TJA1040T CAN transceiver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the internal resistance of the TJA1040T CAN transceiver?

811 Views
joophliu
Contributor III

Hi Supporter:

      What is the internal resistance of the TJA1040T CAN transceiver? I have checked the datasheet, it have two parameters(common-mode input resistance and differential input resistance).

      What is the understanding of this parameter in the red box below? Does it refer to the internal matching resistance of the CAN transceiver or the external one? What parameter does this percentage refer to?

pastedImage_5.png

Tags (2)
0 Kudos
Reply
1 Reply

763 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:Ri(cm) is resistance between input terminals and GND.

2: Ri(cm)m refers to typical 25K.

3: Ri(df) is resistance between two input terminals .

0 Kudos
Reply