I'd like to overlay widget on camera captured image renderd by gstreamer.
I tried to set X_OVERLAY of mfw_v4lsink element to application widget by gst_x_overlay_set_render_rectangle.
Captured image overlayed on the widget for video display.
then, I add another widget which overlayed on the video display widget.
However, I could not operate the addtional widget.
This problem didn't occur in using ximagesink.
Does anyone know about this?
The application created by using Qt, gstreamer, mfw_v4lsrc and mfw_v4lsink elements.
Device : i.MX6 SABRE Smart Device (Dual Lite)
Platform : Yocto Linux
kernel version : Linux-3.0.35-4.1.0+yocto+gbdde70
Software Changes : X11, Qt framework(ver 4.8.5), gstreamer (ver 0.10.36),
gstreamer fsl plugin (ver 3.0.8) installed.
additional : self-make Qt and gstreamer based application
application
Hardware Changes : no
Frequency of : always
reproducibility
Display type : HDMI(Touch Display on SABRE board) resolution 1024x768
Please see the following thread,
I saw the following information:
does xvimagesink work on fsl-image-gui image ?
fsl-image-gui in xvimagesink, do you really use ?
I have a quetion.
I'm using the daisy.(daisyis revision of yocto)
However, in daisy, fsl-image-gui is build error.
---- build error ----
$ MACHINE=imx6qsabresd source setup-environment build
$ bitbake fsl-image-gui
「ERROR:Nothing PROVIDES 'fsl-image-gui'. Close matches:
fsl-image-multimedia」
Do you know a solution for this error?
Did you do repo sync before doing the bitbake command?, make sure you are using meta-fsl-bsp-release.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------