What is the difference between A0 & B0 Silicon Revisions of IMX8QX Processor ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between A0 & B0 Silicon Revisions of IMX8QX Processor ?

Jump to solution
3,982 Views
rvalvekar
Contributor III

Hello Everyone, 

I have been trying to search extensively for the difference between the Silicon Version of IMX8 Processors. I am unable to find a concrete information about this revision change.

Where would be a good place to get this information ? 

Also does the Revision Change affect the bootloader, the scu-firmware and the arm trusted firmware ? Since then the revisions will also affect the flash.bin container.

Thank You for the support and information.

0 Kudos
1 Solution
3,363 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rohan

B0 fixed some errata and implemented various performance and design changes.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
3,364 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rohan

B0 fixed some errata and implemented various performance and design changes.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,363 Views
dhty2015
Contributor II

Hello Igor,

Now the provided image can no longer be used directly in A0 version. What configuration should I modify if I compile it myself?

0 Kudos
3,363 Views
rvalvekar
Contributor III

Hello Igor,

Thank you for Your assistance and support. 

0 Kudos