What is the TEMPSENSOR_RESERVE pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the TEMPSENSOR_RESERVE pin?

571 次查看
thomaskofoedhan
Contributor III

Can't find any description of the TEMPSENSOR_RESERVE pin. Is it a power or IO pin, what is it used for and what to do with it?

Thomas

标签 (1)
0 项奖励
2 回复数

451 次查看
jamesbone
NXP TechSupport
NXP TechSupport

The pin  TEMPSENSOR_RESERVE  need to be floating,  there is no connection for this terminal, it is part of the Temperature sensor that contains the i.MX7 that it is enable using the pin terminals TEMPSENSOR_REXT which needs to have a 100ohms resistor tie to ground, and the VDD_TEMPSENSOR_1P8 which it is the power terminal for the sensor.

Here is the datasheet for your convenience:

http://www.nxp.com/files/32bit/doc/data_sheet/IMX7SCEC.pdf 


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

451 次查看
thomaskofoedhan
Contributor III

Thank you for your answer and the datasheet. I already have the datasheet although for the dual type, but the only mention of this pin is under the chapter describing what to do with pins if the functionality is NOT used. But in this case this pin is always to be left floating.

0 项奖励