Weston repaint frequency?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Weston repaint frequency?

1,778件の閲覧回数
woutervh
Contributor IV

Hello all,

I seem to have an issue, that whatever I try to run on my weston backend, I never seem to exceed +- 40fps. 

That can also be seen by running the weston-simple-egl test.

When I run weston-simple-egl -f, so fullscreen, I get upto 27 fps.

But, when I add -b, so weston-simple-egl -f -b (Don't sync to compositor redraw (eglSwapInterval 0)), I get a stunning 175 fps!

So what is limiting the weston refresh rate? I'm running on a IMX6D, industrial grade, morty yocto, weston/wayland 1.11. My fb settings are:

mode "1920x1080-60"
# D: 148.500 MHz, H: 67.500 kHz, V: 60.000 Hz
geometry 1920 1080 1920 2160 16
timings 6734 148 88 36 4 44 5
accel false
rgba 5/11,6/5,5/0,0/0
endmode

ラベル(5)
タグ(3)
0 件の賞賛
返信
1 返信

1,477件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Wouter,

There is no limit, that depent of the application, but if you use eglSwapInterval you get max 60fps.

0 件の賞賛
返信