Wayland input method support v3 for BSP 5.15.52_2.1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wayland input method support v3 for BSP 5.15.52_2.1.0

1,039件の閲覧回数
hankwang
Contributor V

Hey, we have a question about the input method of Wayland , we have an application running on Weston using GTK. As far as we know, GTK supports text input protocol v3.

Now we want to transfer characters to the application using the on-screen keyboard. But wayland's input method does not support v3 version. Now the input method only supports v1 version.

Can we know when input-method will support v3 version? Or do we have other ways to send characters to the application?

https://source.codeaurora.org/external/imx/wayland-protocols-imx/tree/unstable/input-method?h=waylan...

4 返答(返信)

678件の閲覧回数
dar_tad
Contributor I

Hello, are there any updates on the topic? I'm developing a Gtk app on an embedded device with Weston, and I would need an on-screen keyboard for user input

0 件の賞賛
返信

1,021件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Sorry in this case you will have to wait until next releases.

Regards

661件の閲覧回数
hankwang
Contributor V

OK. We got it.

655件の閲覧回数
dar_tad
Contributor I

Hi,

Could you please explain this to me? 

0 件の賞賛
返信