Watchdog doesn't work at 400Mhz set point on IMX6SL custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog doesn't work at 400Mhz set point on IMX6SL custom board

623 Views
RobHawksFan
Contributor I

I have a custom board that has a IMX6SL. The design is based on the IMX6SL-EVK design. My board has a PMIC and is running in LDO bypass mode. The watchdog reset seems to work perfect as long as I run  the board at 1Ghz or 800 Mhz. When i manually set the CPU to 400Mhz (cpufreq-set -f 400000) and then try to issue a reset command from w/i linux the watchdog nolonger works. System hangs and I get "Watchdog reset failed to assert reset". Anyone else expierence this problem?  Why does it work at  1Ghz & 800Mhz but not 400Mhz?

Labels (4)
0 Kudos
Reply
1 Reply

490 Views
igorpadykov
NXP Employee
NXP Employee

Hi RobHawksFan

at 400MHz processor voltages may be lowered, while

at reset processor starts with 792MHz and 400MHz voltage levels

may be insufficient. One can try to reset PMIC too (PWRON)

or boot with 400MHz (set BT_FREQ=1).

Best regards

igor

0 Kudos
Reply