Hi,
I have IMX28EVK . I need to connect a wifi module based on marvell sd 8787(sdio wifi module driver) .
I have linux bsp for imx28 and wfi driver sd8787. Do I have to edit wifi driver files to work with imx28evk?
Do I have to edit any files of bsp source ? Please help me.
thanks
pt
已解决! 转到解答。
Hello, Pt A R
Please see following advice for your porting WIFI to I.MX28 system!
>> Do I have to edit wifi driver files to work with imx28evk?
Yes, you must compile SD8787 driver with cross-compiler that released with i.mx28 linux BSP(LTIB), In order to debug wifi conveniently, you had better compile wifi driver to be module(.ko file), Then use command line to load SD8787 driver.
# insmod sd8787.ko "here is firmware"
Note: except for driver for 8787, you should also have firmware give by marvell, I recommand you contact marvell or distrabutor and get corresonding documents about SD8787 linux porting.
In addition, you also need to check if SD pins for WIFI have been iomuxed in BSP file, if not, add them ,please!
>> Debuging wifi in linux system
Let me introduce some tools for wifi debuging in linux.
(1)iwconfig
(2)wpa_supplicant
(3)wpa_cli
configuration file is : wpa_supplicant.conf
On how to debug wifi by using above tools on linux platform, you can get much more information from internet, so please search them and learn how to use them.
Regards,
Weidong
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.
For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )
Thank you for using Freescale Community.
Hello, Pt A R
Please see following advice for your porting WIFI to I.MX28 system!
>> Do I have to edit wifi driver files to work with imx28evk?
Yes, you must compile SD8787 driver with cross-compiler that released with i.mx28 linux BSP(LTIB), In order to debug wifi conveniently, you had better compile wifi driver to be module(.ko file), Then use command line to load SD8787 driver.
# insmod sd8787.ko "here is firmware"
Note: except for driver for 8787, you should also have firmware give by marvell, I recommand you contact marvell or distrabutor and get corresonding documents about SD8787 linux porting.
In addition, you also need to check if SD pins for WIFI have been iomuxed in BSP file, if not, add them ,please!
>> Debuging wifi in linux system
Let me introduce some tools for wifi debuging in linux.
(1)iwconfig
(2)wpa_supplicant
(3)wpa_cli
configuration file is : wpa_supplicant.conf
On how to debug wifi by using above tools on linux platform, you can get much more information from internet, so please search them and learn how to use them.
Regards,
Weidong
done the following ...
a) Copy firmware image sd8787_uapsta.bin | ... to
/system/etc/firmware/mrvl/ directory, create the directory if it doesn't exist.
b) Install WLAN driver,
For example, to install SD8787 driver,
insmod mlan.ko
insmod sd8787.ko
but not recognizing wifi module.please help.
in which file should i edit to make sd pin iomuxed?
Hi weidong.sun,freescale-admin,alejandrolozano,jimmychan,JiangJustin
Evaluation-kit : MCIMXEVK
Linux :2.6.35 version
Wifi driver :MARVELL SD8787
I have the linux-2.6.35 kernel image(build from the L2.6.35_1.1.0_130130_source customized for imx28). I want to install the marvell sd8787 driver to enable my wifi module.I have the following sources...
Wifi driver source available:
1. mlan.ko and sd8787.ko (supports linux2.6.32)
2. imx53-wifi driver source[ didn't use the config file imx53. I have just used the fwImage (sd8787_uapsta.bin),wlan_src file from that source.]
a) which conatins sd8787_uapsta.bin file
b)sd8787/wlan_src - marvell wifi driver source.[have built the mlan.ko and sd8xxx.ko using the source ]
Successfully booting from sd card and logged in as root( freescale login: root).
root@freescale
As per the readme file available with the 2nd source( imx53-wifi driver source ), I have created a directory for the marvell wifi driver( /system/etc/firmware/mrvl/)
and copied the sd8787_uapsta.bin file to it. and then did the following
1.insmod mlan.ko
2.insmod sd8xxx.ko [drv_mode=3] [fw_name=mrvl/sd8787_uapsta.bin]
Thus I installed wlan driver. But wifi module is not recognizing.
Doubts:
I have got the wlan source and sd8787_uapsta.bin file from i.MX53_SD8787_src_Release-1.0 . Are these files are general for imx processors or the sd8787 source is different for each processor? Then where should I have to edit to customize the sd8787 source for imx28? Please help me.
alejandrolozano please check this issue and help me.
Hi Pt A R
I think you can check that smth like sd8787_probe is called in
codes, you need to add init function for sd8787 device in arch/arm/mach-mx28/device.c.
Also one needs to add device for "sd8787_sdio". You can reference all the
other modules init function in device.c how the device is added, such as below.
static void __init mx28_init_pxp(void)
{
struct platform_device *pdev;
pdev = mxs_get_device("mxs-pxp", 0);
if (pdev == NULL || IS_ERR(pdev))
return;
pdev->resource = pxp_resource;
pdev->num_resources = ARRAY_SIZE(pxp_resource);
mxs_add_device(pdev, 3);
}
Best regards
chip
Hi igorpadykov ,
Thanks igorpadykov.
Please check this log. This is what I get when I connect the wifi module.
message log:
mmc1: new high speed SDIO card at address 0001
Enter: mlan_register
Enter: wlan_disable_host_int
Enter: wlan_sdio_disable_host_int_mask
Leave: wlan_sdio_disable_host_int_mask
Leave: wlan_disable_host_int
SDIO FUNC1 IO port: 0x10000
Enter: wlan_init_lock_list
Leave: wlan_init_lock_list
Enter: wlan_init_timer
Leave: wlan_init_timer
Leave: mlan_register
request_firmware() failed, error code = 0xfffffffe
Firmware Init Failed
Enter: mlan_unregister
Enter: wlan_free_timer
Leave: wlan_free_timer
Enter: wlan_free_lock_list
Leave: wlan_free_lock_list
Leave: mlan_unregister
woal_add_card failed
wlan_sdio: probe of mmc1:0001:1 failed with error -1
regards
pt
On iMX28 EVK, to support this 8787 wifi card, in kernel, the followed feature should be built as module. And the firmware should be put to "\lib\firmware\mrvl\sd8787_uapsta.bin"
Kernel config menuconfig
-*- Networking support -->
-*- Wireless -->
<M> cfg80211 - wireless configuration API
$ insmod cfg80211.ko
$ insmod mlan.ko
$ insmod sd8xxx.ko drv_mode=1
$ ifconfig mlan0 up
Hi
Thanks Qiang_FSL.
I am getting this error while using the following command :
#iwconfig mlan0 essid <ap-ssid>
Enter: wlan_is_network_compatible
wlan_is_network_compatible() FAILED: index=0 wpa_ie=0x0 wpa2_ie=0x30 WEP=d WPA=d WPA2=d EncMode=0x0 privacy=0x1
Error for wireless request "Set ESSID" (8B1A) :
SET failed on device mlan0 ; Bad address.
Regards
Pt.
my wireless ap is airtel123. I have used the command -
iwconfig mlan0 essid airtel123
but it says "BAD ADDRESS"
wlan_is_network_compatible() FAILED: index=0 wpa_ie=0x0 wpa2_ie=0x30 WEP=d WPA=d WPA2=d EncMode=0x0 privacy=0x1
Leave: wlan_is_network_compatible
Leave: wlan_find_ssid_in_list
Can not find ssid airtel123
Leave: wlan_find_bss
Leave: wlan_bss_ioctl_find_bss
Leave: wlan_bss_ioctl
Leave: mlan_sta_ioctl
Leave: mlan_ioctl
Error for wireless request "Set ESSID" (8B1A) :
SET failed on device mlan0 ; Bad address.
If you run iwconfig, what will you see?
I haven't get this issue, I used the L2.6.35_1.1.0_ER_iMX28 BSP, the wifi driver version is "SD-UAPSTA-BT-FM-8787-LINUX2632-PXA920-14 57 5 p86-M2614130 p47_AX-GPL". It works fine.
Hi Qiang_FSL, igorpadykov
$ insmod cfg80211.ko throws an error:-
root@freescale /home/user$ insmod cfg80211.ko
cfg80211: disagrees about version of symbol wireless_send_event
cfg80211: Unknown symbol wireless_send_event (err -22)
insmod: can't insert 'cfg80211.ko': Invalid argument
Hi Qiang_FSL
The cfg80211.ko module have built in the same ltib.
we write the file system to sd card using this command
./mk_mx28_sd /dev/sdb
Then use the insmod cfg80211.ko command to install the module.
This is the message log which I get
root@freescale /home/user$ insmod cfg80211.ko
cfg80211: disagrees about version of symbol skb_copy_bits
cfg80211: Unknown symbol skb_copy_bits (err -22)
cfg80211: disagrees about version of symbol rfkill_unregister
cfg80211: Unknown symbol rfkill_unregister (err -22)
cfg80211: disagrees about version of symbol skb_put
cfg80211: Unknown symbol skb_put (err -22)
cfg80211: disagrees about version of symbol consume_skb
cfg80211: Unknown symbol consume_skb (err -22)
cfg80211: disagrees about version of symbol rfkill_blocked
cfg80211: Unknown symbol rfkill_blocked (err -22)
cfg80211: disagrees about version of symbol rfkill_destroy
cfg80211: Unknown symbol rfkill_destroy (err -22)
cfg80211: disagrees about version of symbol genlmsg_multicast_allns
cfg80211: Unknown symbol genlmsg_multicast_allns (err -22)
cfg80211: disagrees about version of symbol pskb_expand_head
cfg80211: Unknown symbol pskb_expand_head (err -22)
cfg80211: disagrees about version of symbol kfree_skb
cfg80211: Unknown symbol kfree_skb (err -22)
cfg80211: disagrees about version of symbol netlink_broadcast
cfg80211: Unknown symbol netlink_broadcast (err -22)
cfg80211: disagrees about version of symbol __alloc_skb
cfg80211: Unknown symbol __alloc_skb (err -22)
cfg80211: disagrees about version of symbol rfkill_resume_polling
cfg80211: Unknown symbol rfkill_resume_polling (err -22)
cfg80211: disagrees about version of symbol kobject_uevent_env
cfg80211: Unknown symbol kobject_uevent_env (err -22)
cfg80211: disagrees about version of symbol __dev_get_by_index
cfg80211: Unknown symbol __dev_get_by_index (err -22)
cfg80211: disagrees about version of symbol skb_pull
cfg80211: Unknown symbol skb_pull (err -22)
cfg80211: disagrees about version of symbol genl_register_family_with_ops
cfg80211: Unknown symbol genl_register_family_with_ops (err -22)
cfg80211: disagrees about version of symbol rfkill_pause_polling
cfg80211: Unknown symbol rfkill_pause_polling (err -22)
cfg80211: disagrees about version of symbol netlink_unicast
cfg80211: Unknown symbol netlink_unicast (err -22)
cfg80211: disagrees about version of symbol dev_get_by_index
cfg80211: Unknown symbol dev_get_by_index (err -22)
cfg80211: disagrees about version of symbol dev_close
cfg80211: Unknown symbol dev_close (err -22)
cfg80211: disagrees about version of symbol skb_push
cfg80211: Unknown symbol skb_push (err -22)
cfg80211: disagrees about version of symbol wireless_send_event
cfg80211: Unknown symbol wireless_send_event (err -22)
cfg80211: disagrees about version of symbol nla_put
cfg80211: Unknown symbol nla_put (err -22)
cfg80211: disagrees about version of symbol rfkill_set_hw_state
cfg80211: Unknown symbol rfkill_set_hw_state (err -22)
cfg80211: disagrees about version of symbol ethtool_op_get_link
cfg80211: Unknown symbol ethtool_op_get_link (err -22)
cfg80211: disagrees about version of symbol rfkill_alloc
cfg80211: Unknown symbol rfkill_alloc (err -22)
cfg80211: disagrees about version of symbol dev_alloc_skb
cfg80211: Unknown symbol dev_alloc_skb (err -22)
cfg80211: disagrees about version of symbol __pskb_pull_tail
cfg80211: Unknown symbol __pskb_pull_tail (err -22)
cfg80211: disagrees about version of symbol skb_trim
cfg80211: Unknown symbol skb_trim (err -22)
cfg80211: disagrees about version of symbol rfkill_register
cfg80211: Unknown symbol rfkill_register (err -22)
cfg80211: disagrees about version of symbol dev_change_net_namespace
cfg80211: Unknown symbol dev_change_net_namespace (err -22)
cfg80211: disagrees about version of symbol rfkill_set_sw_state
cfg80211: Unknown symbol rfkill_set_sw_state (err -22)
insmod: can't insert 'cfg80211.ko': Invalid argument
In your kernel ".config" file, you should make sure the followed wireless config:
CONFIG_WIRELESS=y
CONFIG_WIRELESS_EXT=y
CONFIG_WEXT_CORE=y
CONFIG_WEXT_PROC=y
CONFIG_WEXT_SPY=y
CONFIG_WEXT_PRIV=y
CONFIG_CFG80211=m
# CONFIG_NL80211_TESTMODE is not set
# CONFIG_CFG80211_DEVELOPER_WARNINGS is not set
# CONFIG_CFG80211_REG_DEBUG is not set
CONFIG_CFG80211_DEFAULT_PS=y
# CONFIG_CFG80211_DEBUGFS is not set
# CONFIG_CFG80211_INTERNAL_REGDB is not set
CONFIG_CFG80211_WEXT=y
CONFIG_WIRELESS_EXT_SYSFS=y
CONFIG_LIB80211=y
# CONFIG_LIB80211_DEBUG is not set
# CONFIG_MAC80211 is not set
Hi Qiang_FSL
in my kernel .config file ,
/* wireless configuration */
CONFIG_CFG80211_DEBUGFS =y
CONFIG_LIB80211 is not set
CONFIG_MAC80211=m
except these three other configs are same as in your reply
Now I alter the config to ...
CONFIG_CFG80211_DEBUGFS is not set
CONFIG_LIB80211 =y
CONFIG_MAC80211 is not set
This time also I am getting the error as:
root@freescale /home/user$ insmod cfg80211.ko
cfg80211: disagrees about version of symbol wireless_send_event
cfg80211: Unknown symbol wireless_send_event (err -22)
insmod: can't insert 'cfg80211.ko': Invalid argument
In kernel config menu, Device Drivers -> Network device support -> Wireless LAN, please make sure AR600x driver is enabled.
<M> Atheros AR600x support (non mac80211)
Maybe you can attach your ".config" here.
Compared your config file, I havne't enabled "CONFIG_LIB80211=m".
By the way, I think you can try with WiressAP which has no password first. For iwconfig, as I know the password parameters should be in hex format, not the text you set in AP.