Hi all,
We are developing a system which has Miracast functionality in i.MX6 platform.
Thanks to the Freescale's libfsl_wfd.so, we are able to connect all Nexus devices as a WFD source.
FYI, our system runs as a WFD sink.
But when I try to connect to our MX6 device from non-Google devices such as Galaxy S3/S4, I got the following messages;
E/WifiDisplaySink( 1478): Invalid server_port description '19000'.
F/WifiDisplaySink( 1478): frameworks/imx-wfd/jni/sink/WifiDisplaySink.cpp:508 CHECK_EQ( err,(status_t)OK) failed: -1007 vs. 0
F/libc ( 1478): Fatal signal 11 (SIGSEGV) at 0xdeadbaad (code=1), thread 2463 (ALooper)
Do you have any ideas to use non-Google devices?
Thanks in advance!
Hi,
Yong
Which Wi-FI module are you using?