I want cross compile Qt5.6 to imx6sx with yocto, after bitbake fsl-image-qt5, i got these warnings
WARNING: lttng-modules: no modules were created; this may be due to CONFIG_TRACEPOINTS not being enabled in your kernel.
WARNING: QA Issue: devil rdepends on tiff, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: devil rdepends on liblzma, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: The /usr/share/info/dir file is not meant to be shipped in a particular package. [infodir]
WARNING: QA Issue: qtbase-plugins rdepends on freetype, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase-plugins rdepends on fontconfig, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase rdepends on freetype, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase rdepends on libicui18n, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase rdepends on fontconfig, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase rdepends on libicuuc, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: imx-gpu-viv: /imx-gpu-viv-tools/usr/bin/gmem_info is owned by uid 1000, which is the same as the user running bitbake. This may be due to host contamination [host-user-contaminated]
WARNING: QA Issue: imx-gpu-viv: /imx-gpu-viv-tools-apitrace/usr/lib/apitrace/wrappers/egltrace.so is owned by uid 1000, which is the same as the user running bitbake. This may be due to host contamination [host-user-contaminated]
when i burn u-boot,zImage and rootfs to imx6 and run the qt demo, Segmentation fault is display,like this :
file:///usr/share/qt5everywheredemo-1.0/qml/QtDemo/main.qml:124:5: QML FontLoader: Cannot load font: "file:///usr/share/qt5everywheredemo-1.0/qml/QtDemo/fonts/PatrickHandSC-Regular.ttf"
Segmentation fault
please help me out,thanks a lot!
已解决! 转到解答。
Hi Bio_TICFSL,
i can avoid these warnings by append freetype fontconfig uic these things to RDEPENDS and DEPENDS in source/meta-qt5/recipes-qt/qt5/qtbase_git.bb,but when i run the qt demo,Segmentation fault still there.:smileysad:
Hi Chen,
I guess you should start to fix the host contamination issue: https://patches.openembedded.org/patch/124085/
then fix all that QT dependencies: [OE-core] What does "QA Issue: ... rdepends on .. but its not a build dependency?" mean
segmentation fault is due to memory issues, I suggest to fix firts all that depencies issues then focus on segmentation fault.
regards
Hi Bio_TICFSL,
i can avoid these warnings by append freetype fontconfig uic these things to RDEPENDS and DEPENDS in source/meta-qt5/recipes-qt/qt5/qtbase_git.bb,but when i run the qt demo,Segmentation fault still there.:smileysad: