Hi, All.
Below circuit is designed refer to SABRE Bd of i.MX6DL.
I wonder about 'Maximum level' of 'LICELL' about 'MMPF0100NPAZES.'
Because charging voltage of 'LIR2450(Li-on Battery)'is '4.2V.'
So, I'll set output level of 'U4(LT3012HFE#PBF)' is '4.2V.'
But see the datasheet of 'MMPF0100NPAZES', max. level of 'LICELL' is 3.6V like below.
I think ordinary li-on battery of charging level is '4.2V.'
So,I want to know that it is possible to use '4.2V' level for 'LICELL' of 'MMPF0100NPAZES'.
Please, Inform me about that questions, ASAP.
Best Regards,
Inho Jeon
Hello,
The MMPF0100 Datasheet is correct : maximum allowed LICELL voltage is 3.6 V.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------